Other Parts Discussed in Thread: UCC27712,
Hi, I would like to use the UCC37324 chip to power or drive a PMSM that we have design. However, we need to develop a specific design since the motor is a dual-stator with different winding inductance. We like this chip because it's a DIP format. However, I'm not expert enough to determine if this chip, will be able to handle up to 250Vdc link on the MOSFETs or IGBTs sides, I was unable to find any information on this matter. For example, it's very clear in the data sheet of the UCC27712.
Also, since the UCC37324 seams to have no boostrap and if it's capable to be use in an inverter, then the inverter would need to be driven-design in bipolar scheme, right?
Thanks,
Donald W.
Openvolta project