This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

no

i have to fast switch between -5 volts and -3.2 volts. i need 150 mA to 300 mA current at output. kindly suggest any component to do the job.

  • Hello Malik,

    Do you have -5V and -3.2V already available, and need a semiconductor switch to alternate between them?
    Or do you need to create a -5V and -3.2V from some other source and then quickly change the Vout of this converter?