Other Parts Discussed in Thread: BQ25155
Hi team,
My customer would like to use BQ24081-Q1 to achieve below functions.
- Max charge current to 250mA when battery temperature is -20 to +50C
- Max charge current need to limit to 20mA when battery temperature is -40 to +85C
Is it possible to achieve? (I think the problem is ISET resistance can be changed dynamically or not?)
If BQ24081-Q1 can't do, may I have your help to recommend other parts?
Below are the requirements.
1. Vin = 5V.
2. Charge current = 250mA max.
3. 1S2P Li-ion battery.
4. AEC-Q100 needed.
Thank you.
Regards,
Allen