This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92513HV: Max PWM frequency and RT/CLK Pin

Part Number: TPS92513HV

Hello team,

my customer is using the TPS92513HV and is considering in using it in a new redesign. The concerns are two:

- Maximum signal frequency applicable on the PWM dimming input pin:
On the datasheet it shows only the nominal parameter of t_rise, t_fall.
On the chapter "8.3.5 PWM Dimming (PDIM Pin)" of the same datasheet reports the note "The dimming frequency range is 100Hz to 1kHz", while on the application note TIDUBW3A (https://www.ti.com/lit/ug /tidubw3a/tidubw3a.pdf) in the chapter "2.2.2 Digital PWM Dimming Using PDIM" is the note "The dimming frequency range is 200 Hz to 5kHz".
To date the tested products approved and in mass production work at 2.4kHz.
I would like to know if there are any contraindications and attentions to keep to upgrade this frequency in the 15kHz-20kHz range.

-Synchronizing the Switching Frequency to an External Clock (RT / CLK Pin):
I would like to know if there are any contraindications and attentions to keep in generating the signal in object from micro controller in order to make the TPS92513HV driver work at different frequencies according to the different load conditions with "slow" transitions of the order of 100mS.
This technique would allow me to expand the V and I working ranges with the same hardware.

Please let me know.

Thank you and best regards,

Adrian

  • Hello Adrian,

    It is not recommended to PWM the TPS92513HV at 15-20 KHz though it may work.  Contrast ratio will be significantly reduced.  Rise and Fall time of the inductor current can cause non-linear dimming and regulation issues.  The recommended range is 100 Hz to 1 KHz, it can be used beyond this with limitations on dimming performance that depend on the design such as Input voltage, Output voltage, switching frequency and inductor value.  The t_rise and t_fall are small compared to the current slew rate of the inductor.

    The TPS92513HV can work this way.  It takes time for the TPS92513HV to switch from RT switching frequency to external synchronized switching frequency.  It has to meet the criteria below.  Is this a dynamic change or something set once the load conditions are known?  This would be something to try and see how it behaves when implementing this.  I would look at current regulation to make sure it remains stable due to changing ripple current.  Also, as stated below, switching in and out of this mode is not desirable since the converter drops switching frequency to 150 KHz which can cause issues in some designs (designs intended for higher switching frequency).  The sync capacitor and resistor are also needed as stated below and is shown in Figure 12 of the datasheet.

    From the datasheet:

    8.3.3 Synchronizing the Switching Frequency to an External Clock (RT/CLK Pin)
    The RT/CLK pin can be used to synchronize the regulator to an external system clock by connecting a square
    wave to the RT/CLK pin through the circuit network as shown in Figure 12. The square wave amplitude must
    transition lower than 0.63 V and higher than 1.81 V on the RT/CLK pin and have an on-time greater than 51 ns
    and an off-time greater than 100 ns. The synchronization frequency range is 300 kHz to 2 MHz. The rising edge
    of the PH is synchronized to the falling edge of RT/CLK pin signal. The internal oscillator provides default
    switching frequency set by connecting the resistor from the RT/CLK pin to ground should the synchronization
    signal turn off.

    It is required to AC couple the synchronization signal through a 470 pF ceramic capacitor and a 4 kΩ series
    resistor to the RT/CLK pin. The series resistor reduces PH jitter in heavy load applications when synchronizing to
    an external clock and in applications which transition from synchronizing to RT mode. The first time the RT/CLK
    pin is pulled above the CLK threshold the device switches from the RT resistor frequency to PLL mode. The
    internal 0.5 V voltage source is removed and the CLK pin becomes high impedance as the PLL starts to lock
    onto the external signal. Since there is a PLL on the regulator, the switching frequency can be higher or lower
    than the frequency set with the external resistor. The device transitions from the resistor mode to the PLL mode
    and then increases or decreases the switching frequency until the PLL locks onto the CLK frequency within 100
    microseconds.
    When the device transitions from the PLL to resistor mode, the switching frequency slows down from the CLK
    frequency to 150 kHz, then reapplies the 0.5 V voltage and the resistor then sets the switching frequency. It is
    not recommended that a system transition from PLL mode to resistor mode repeatedly during operation. When
    the PLL loses the external clock input the default 150 kHz switching frequency creates long on-times, which
    result in higher inductor ripple currents. This can lead to inductor saturation if the system is not designed to
    operate at this frequency.

    Best Regards,