Hello:
I am using 2x Li 3.6V cell in parallel. With a low dropout cutoff of around 2.0V, I need to get 8V from a boost regulator. The "idle" current is < 100mA, but a "peak" current of about 800mA is required for about 300ms during a transmit sequence. Webench says the best I can get is about 400mA. From what information I can gather, I believe I need a supercap to provide the missing short duration energy. I have not done those calculations yet, but I'm sure there are various sizes and combinations of caps to fill that energy gap.
Does it make sense to use it on the input side, or output side? If either could be used, why is one better than the other? Can someone provide a link to a design that might use such an arrangement? Why does webench not have the option to use a supercap? (asking a bit much maybe?)
Thanks!