Hello,
I am planning to use BQ21040 to charge a battery. This battery has an internal NTC I will connect to the TS pin.
I would like to use the same NTC to do another temperature measurement.
As I see in the datasheet, BQ21040 biases the NTC with a current source, 50uA if charging, 30uA if charge disabled (I guess when temp>45C).
I can work with it but, what happens in the TS pin if Vin<4.45V?
If ntc is not biased in that case, can I bias the NTC from the other device? (I would be setting a voltage on TS pin then)
Is there any other situation where BQ21040 does not bias the NTC?
Regards,
Dave