This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61199: The relation between OVP and LED bar Vf

Part Number: TPS61199

Hi

I am using a TPS61199 to make a LED driver board to drive LED bar.

The issue is that I set the OVP=60V, it is OK when the LED bar Vf=54V, however the LED bar will flash if Vf=27V(Reduce the LED quantity).

Is there a limitation between OVP setting and real LED bar Vf?