Part Number: LM5164-Q1
Hi,
Im intrested to know if this buck converter can be configured to provide a negative output (-15V) when the supply is +48Vdc. I have been able to achive this with other buck designs advice is welcomed with this device.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5164-Q1
Hi,
Im intrested to know if this buck converter can be configured to provide a negative output (-15V) when the supply is +48Vdc. I have been able to achive this with other buck designs advice is welcomed with this device.
Karl,
Yes you can use the LM5164-Q1 in an inverting buck-boost topology. You've designed these before so you're probably familiar with this app note, "Using a buck converter in an inverting buck-boost topology." This app note explains the considerations of the chosen buck and details the operation of the topology.
-Sam
Karl,
Do you have a simulation AND a PCB? Which does not work?
Simulations often do not work for inverting-buck-boost because the GND pin can be internally connected to system GND. If the sim is not working, this may be the issue.
If the board is not working, does the sim work?
Thanks,
-Sam
(Hi Sam,
I have a TI evaluation board (LM5164-Q1EVM-041 Converter Evaluation Module) that was initially tested as +12V output. I then hacked the evaluation board to isolate components and connections from ground in order to enable the grounding of the positive output. Which should have caused the isolated circuit that was previously grounded to go negative (-12V).
However there appers to be no output when configured in such a way.
Regards
Karl
Karl,
You should be able to take the unmodified EVM and connect Supply+ to VIN and Supply- to VOUT to get an inverting buck boost where the GND pin of the IC is now considered -VOUT and the VOUT of the buck converter is now GND. You may need to add a capacitor from VIN to VOUT (of the buck, GND of the inverting buck boost) but you should not need more modifications than that.
If you have an unmodified EVM, you can try that. Or you can put the EVM back in its original state and try.
-Sam
Karl,
I have not heard back. Are you still having trouble getting this to work? If so, please let me know.
Thanks,
-Sam