I have a 10 cell pack capable of delivering 100A at 37V, and a system with a max load of 1kW. I'm designing a BMS using the BQ76930 and based on current consumption needs, I chose a 2mOhm RSENS. I need to set my OCD to trip at 70A, but that means OCD is 140mV, and this chip's highest rating is 100mV. Is there a better BSM chip out there to handle this value? it seems that the OCD levels for this series are all the same... Or is there something I missed?
Further, when I clicked the link to get the SLUCC539 programming software, the page is missing.