Other Parts Discussed in Thread: LP8555, TPS61199
Hi,
My customer is having below questions:
PWM pin is used for dimming mode control, so frequency is from 100Hz to 22K.
In our application, we use direct PWM as LED one/off control, so IC might work as low as 60Hz.
Can you help to check if using directly PWM mode, can we use 60~120Hz 5% duty for this IC?
Please let us know if there are further information needed.
Thanks a lot.