This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/BQ34110: Bq34110

Part Number: BQ34110
Other Parts Discussed in Thread: BQSTUDIO

Tool/software: TI C/C++ Compiler

Dear sir / mam

 i have done with system to configuration for Alert generation .

following these steps.

1. Manufacturing Status Init.

  configuration data  in data flash is 0x001F at register 0x40D7

2. Alert1_0 Config -> register 0x413E -> value set 0x01

3.  Alert2_0 Config -> register 0x4145 -> value set 0x01

and i read the BatteryStatus() 0x0A/0x0B. and check signal in Alert pin.

Apply voltage by Battery 1 - 11.04 and other battery has 6.5 v . i have operate >5V operation.

but Alert interrupt has not generated.

so please help me.