This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Debounce delay on Emergency FET SHUTDN pin

Part Number: BQ40Z80

Hello,

I am hoping that I can configure the debounce delay within the Data Memory section of the bq40z80.

This is in regards to the Emergency FET SHUTDN pin that I am using as an ON/OFF switch for system power.  As it stands, the pin has a built in 1 second debounce delay.  (i.e. hold down a momentary push button for 1 second to change the entry or exit of shutdown).  I would like to change this to 3 seconds if possible.   

Is this something that can be configured?

Thank you!

-Chris