Hi Team,
Here is a question from customer.
In customer's application, they use a controller co-work with UCC27211A. And when powering off, UCC27211A will enter into UVLO first, and then the controller enter into UVLO, that means, when UCC27211A enters into UVLO, there is still PWM input. So customer has concern on the output status of UCC27211A at such condtion to see if it affect the total sys. below are some conditions customer can think of and if there is other condition, please kindly also list.
1. PWM is high. For example
a. HI is high and 27211A enter into UVLO, then what's the status of HO? Is it HIGH or LOW?
b. HI is high and 27211A enter into UVLO, then 27211A recovers, what's the status of HO? does it change to LOW when enter into UVLO then go to HIGH when recover?
2. PWM is low. For example,
a. HI is Low and 27211A enter into UVLO, then what's the status of HO? Is it HIGH or LOW?
Looking forward to your reply and thanks.
BRs
Given