Part Number: TPS563209
Other Parts Discussed in Thread: TPS56339, TPS54302, TPS54308
We are using TPS563209 in our design.
This IC is with Fixed Frequency of 650KHz.
While capturing the waveform at SW node of this IC, We observed frequency variation from around 660Khz to 710Khz (Frequency found variation continuously in this range). Why this deviation? Please suggest,
This IC does not specified any frequency dithering.
Due to this variation in frequency, We are facing RF interference with LF RFID. Harmonics of this is getting couple to RFID Harmonics.
We have validated with Fixed DC load of 0.5A, 1A and 2A.
Input to the IC is 12VDC.
Output adjusted to 5V.
Attached are the Waveform at SW node of TPS563209. (In all three load condition, Frequency variation observed)
Load Condition 1 : 0.5A
Load Condition 2 : 1A
Load Condition 3 : 2A