This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Low power Boost converter with integrated LDO or without it

Other Parts Discussed in Thread: TPS61099

I have a input dc voltage range of 3V to 4.2V (Input).

Design looks like this:  Input(3-4.2V)  -> Boost -> LDO -> 4.3V or lower

Edit:- Closer the output voltage of LDO to 4.3V(but not more than 4.3V) better it is, since it will give better adc resolution, have adc reference 4.3V actually.

Need to get 4.3V or lower at the output. LDO is used to remove switching noise for measuring sensitive analog signals.

Entire ckt is battery powered so low power is required. Can you suggest some suitable solution for this?