This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please recommend a boost converter with MTTP

Other Parts Discussed in Thread: TPS61099

Hello,

My application block as below, power source is a solar panel(3V, 2mA~60mA output), I am seeking a boost converter that can increase voltage to 5V, I have tried TPS61099 but the efficiency is around 83% after I evaluated it with EVM, do you have boost conventer with MPPT(max power point tracking)? MPPT may have more efficiency in my case or could you suggest other one? thanks.

webber