Hello Experts,
I have a question as attached file. Would you answer it, please?
Best Regards,
Fujiwara
UCC39002 question(10232019).xlsx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Experts,
I have a question as attached file. Would you answer it, please?
Best Regards,
Fujiwara
UCC39002 question(10232019).xlsx
Hi Yasushi,
For Q1, yes Iout_min is 1mA, the maximum voltage of LS pin is (VDD-1.7V), I think 10V here is reasonable.
For Q2, I am not an expert on our hot swap controllers so I will see if I can get one of my colleagues to answer this question.
Regards,
Teng
Hi Teng-san,
Did you get any answer from your colleagues? I appreciate if you share it. Also, I have one more question. Can UCC39002 use with CHS4004812/CHS7004812H?
Best Regards,
Fujiwara
Hi Fujiwara-san,
Unfortunately the UCC39002 is not suitable for hot swap applications. TI does not have a load share controller that is robust for hot swap applications.
Regards
Peter