i would like to design a Battery management system.
which can Manage battery power and control output Load of Maximum 1300W LED Light.
System output : ~400 VDC
No. of Output channel : 4
Battery type : 18650
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i would like to design a Battery management system.
which can Manage battery power and control output Load of Maximum 1300W LED Light.
System output : ~400 VDC
No. of Output channel : 4
Battery type : 18650
Hi Jay,
We don't have device supports your requirements.
If you give us more details then I can try to direct to right forums.
thanks
roger