This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are currently using LP2950ACZ-5.0. I am thinking to use for diferent application. But I would like to know how much the temperature goes up by Vin=24V, Vout=5V and Iout=100mA.
Please advise.
Hironari
Hi Hironari-san,
With Vin=24V, Vout=5V and Iout=100mA, the LDO is burning (24-5)x 0.1 = 1.9Watts
Depending on what package you have, you may need to use the RthetaJA number to calculate the temperature rise.
For example, if you are using the LP package, the temperature rise is 140 x 1.9 = 266 C. You will also need to add your ambient temperature to calculate the junction temperature. The highest junction needs to be less than 125C. Obviously, this package cannot tolerate such big power.
Regards,
Jason Song
Thank you very much your prompt reply.
I understand what you said.
But I would like to know any altanateve or recomendation from your devise such as DC/DC converter.
Vin=24V, Vout=5V, Iout=100mA are the same.
Can DC/DC prevent the heat up?
BEST REGARDS,
Hironari
HI HIronari-san,
Yes. A DC/DC converter is usually more efficient when you have very large Input-output differences. Here are a few options that you might look into:
I hope this helps.
Regards,