Hello,
I have a question about a safety related issue in an offline flyback converter, I plan to use the UCC28630.
I am evaluating cases with a singular component failure that may expose a user to dangerous voltage levels at the output of a flyback converter with 24 V output voltage and wide range mains input. In case the secondary diode fails and shorts, the mains voltage divided by -Np/Ns of the transformer is applied on the output pins of the converter during the conduction phase of the primary FET. I want to make this safe by putting a second diode that has the cathode at the same place as the rectifier diode and the anode at the "bottom" secondary transformer winding. This diode would get forward biased in above mentioned failure case and activate a fuse which is in parallel with the rectifier diode.
Is this a valid approach, or does the UCC28630 already protect the output from such failures? Similar ICs from e.g. ON (FSQ0565) specifically have protections for these cases (in ON's case: Abnormal Over-Current Protection), but I couldn't read from the UCC28630's datasheet if it features something similar.
Thanks and regards
Alex