Hi
Would you share How to calculate the power dissipation?
In my application,
- there are 4 strings,
- each string has 9 LEDs (VF = 3.7V x 9 )
- Vin 9 ~ 16 V
- 90 mA per channel / string
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sir,
The main power consumption cames from current sink and internal MOFET switching and conduction loss. You can refer to Figure 8 to estimate the power consumption on the current sink and refer to rdson of internal MOSFET to know the conduction loss of FET and you can also estimate the switching loss is same with conduction loss Add all together, you can know the power consumption of the TPS61194.
Regards
Sean