This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: LED connected with FLT pin turn on a moment during power on/off

Part Number: TPS2660

Hello experts,

I got question from customer.
My customer plan to use TPS26601 for their system.
They plan to indicate error with LED connected with FLT pin, when TPS26601 detect error (Over current, over VPORR).
But, LED turn on a moment during power on/off timing. They don’t want to turn on LED during power on/off timing.
TPS26601 may detect inrush current during power on timing. Or, this IC may detect V(PORR) error during power off timing.
Do you have any idea to avoid this phenomenon which LED turn a moment on during power on/off?
LED cirsuit is as below;
FLT pin -> resistor (15kohm) -> chip LED
IN pin is connected with UVLO pin directly.
OVP pin and RTN pin are connected directly, also ILIM pin is connected through RLIM with this line.
Thanks and best regards,
Ryo Akashi