Hi,
When TPS65311-Q1 's buck 1 is configured to output 3.3V, what's the maximum current of Buck 1 which can be achieved with 4-40V input?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When TPS65311-Q1 's buck 1 is configured to output 3.3V, what's the maximum current of Buck 1 which can be achieved with 4-40V input?
Thanks.
Hi,
maximum load on BUCK1 mostly depends on the external components like external switching FETs, current sense resistor, temperature conditons, output capacitor and so on. So, it is difficult to make the generic statement. But I have tested it up to 6A at 85C and up to 18V and it works very well.
Regards,
Murthy