This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: About crossover frequency.

Part Number: TPS54302

Equation 14 states that it should be 40kHz or lower, but if C6 is present, can it be 40kHz or higher?

I want to use Cout = 44uF and Vout = 1.15V(R2=10kΩ).
→fo=100.8kHz.
Is it okay if C6 is around 1579pF?