This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: BQ78350-R1 - 0x2B HostFETControl command failure

Part Number: BQ78350-R1
Other Parts Discussed in Thread: TMS320F28062,

Hello,

Recently I have faced to an issue executing 0x2B HostFETControl operation (TMS320F28062 is a host MCU). Symptoms is very likely as described in https://e2e.ti.com/support/power-management/f/196/p/537624/1959380#  topic:

1. I2C speed is 100K. I2C communication is OK (There are several well running devices on the bus).

2. All other BQ78350-R1 commands are executed normally.

3. I run several experiments to put delays before, between and after pair of commands (0x2B, 0x97, 0x11 and 0x2B, 0x00 / 0x01) and that did not help.

4. For testing purposes I also left only HostFETControl commands in code to isolate it from other BQ78350-R1 commands. This did not help as well.

Unfortunately there is no solution in the topic pointed above - any ideas to fix this problem?

Best regards,

Anton