This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: How to create df.fs and bq.fs files?

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO, BQ40Z50,

Hi Guys,

I would like to do production programming of bq40z50 and bq78350-R1 fuel gauges with the bq.fs and df.fs file formats. I have bqStudio v1.3.93. I have the utility to create an SREC, but I don't see anything that generates bq.fs and ds.fs files. 

How do I export these files from an existing gauge?

Thanks!!

Phil

  • Hi Phil,

    There is currently no support for flashstream for the BQ78350-R1 in BQStudio. The srec is the only file that can be generated.

    I think this feature may be in place for the BQ40Z50 under the Firmware tab in BQStudio.

    Best regards,

    Matt