This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am going to use this chip to boost voltage from 12V. I like the output to be in the range from 12V to 15V by using a potentiometer to adjust Feedback voltage. Is it possible?
Thanks,
Xiaoming
Hi Xiaoming:
As the diode will have a voltage drop, so actually the converter still need switching.
What's more, for TPS55330, even there is a minimum on-time limitation as 77ns (typical). If the on-time smaller than the limitation, it will enter into skip pulse operation. Details could be check "7.3.3.1" in datasheet.
So, it could support Vin=12V, Vout=12V, if other conditions are within the recommendation range.
Hi Xiaoming:
As long time not hear you, I assume you have solved the issue. I'll close this post.
If not, just reply below. Thank you~