This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131-Q1: TPS65131 - Load Distance and Stabilization

Part Number: TPS65131-Q1
Other Parts Discussed in Thread: TPS65131

Hello:

I am planning on using the TPS65131TRGERQ1 device in a design, and will of course follow the evaluation module's recommended design and other recommendations. The output will be +12V / -12V, driven with a 3.6V / 17Ah Lithium cell.

The load the supply will be connected to is about 18 inches from the enclosure that houses the supply. With this in mind, is there anything I need to design in to help insure stability of the supply? I expect the current to be about 125mA maximum on either side. I would do the typical things like use twisted pair wiring. Would additional capacitance be of any benefit, provided the ESR is appropriate for the design?

Thanks for any feedback on this you can provide.

Gary