This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2482: Large offset in shunt measurement from Vin

Part Number: TPS2482
Other Parts Discussed in Thread: LM5066I

Hello. I am seeing a large offset voltage on the Shunt Voltage measurement register at no load. With a 1.5m ohm sense resistor, Vin of 24V, and IC output disabled the shunt voltage is measured at 275uV. This corresponds to a 182mA offset current.

I have three ICs on my board and they all show similar offsets. Changing the sample time and averaging does not improve the offset. However, the offset does appear to be dependent on the input voltage level.

Decoupling the input voltage and the logic rail (3.3V) going to Vs allowed me to ramp the input voltage at no load and observe the offset. Below are some sample values:

Vin: 28.454V
ADC Measurement: 0.220A

Vin: 24.006V
ADC Measurement: 0.185A

Vin: 12.395V
ADC Measurement: 0.095A

Vin: 05.596V
ADC Measurement: 0.043A

Vin: 03.309V
ADC Measurement: 0.023A

Is this behavior expected for the device? The amount of error I'm seeing does not match the stated worse-case CMRR in the datasheet but it's possible I'm missing another error source.