This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40170: Inrush current question

Part Number: TPS40170

Dear Sir.

When we were testing the system, we found that we measured the inrush current about 13A.

(The voltage is blue, when the voltage has not reached steady state)

The R (LDRV) resistance set by the TPS40170 is 10K, and the table comparison is 3A.

I would like to ask if there is a chance that the currently measured inrush will cause IC danger or cause no output?