Dear Team,
Can this device support two channel 1V/20A, 0.8V/10A ?
What is the maximum current and voltage for each rail?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Can this device support two channel 1V/20A, 0.8V/10A ?
What is the maximum current and voltage for each rail?
BR
Kevin
Kevin,
Yes this will work. The LM5143-Q1 supports voltages as low as 0.6V and currents as high as 40A per rail.
-Sam