This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561-R1: Fuel Gauge Operation

Part Number: BQ27Z561-R1


Hi Team,

My customer has a question on the BQ27Z561-R1 that I'd like to run by you just to confirm--

For the battery profile, is it saved as non-volatile memory format on the fuel gauge of the battery pack? If so, when the battery is completely drained, will the battery profile be lost? If that's the case, then will the gauge need to be re-programmed and configured by a host MCU?

Looking at the block diagram for this device, it appears the gauge is flash-based so it should retain the battery profile even if the battery is depleted. Can you confirm this is true? Are there any other parameters that need to be programmed to the gauge if it were to loose power completely?

Thanks,
Mitchell