This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All:
I received the question from my customer.
The LM3424 are implemented the high side current sense function.
Can this current sense use as low side current such as following ?
in my customer application, they must put the sample resistance on the low side, if the LM3424 can't meet the function , can i add extra circuit to implement the needs?
or can you suggest other IC to meet the application? Thanks
Hello,
You cannot implement low side current sensing with the LM3424. Please look into using the TPS92691 for low side current sensing.
Thanks Tuan
Hello,
You can attempt to implement that if you meet all of the LM3424 requirements. We do not recommend that if you are not familiar with the part and external design requirements. We recommend you look at the TPS92691.
Thanks Tuan