This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51216: Output Capacitors conditions and Rtrip range

Part Number: TPS51216
Other Parts Discussed in Thread: TPS51716, , TPS51916

Hello

I have two questions about TPS51716.

Q1:About Output Capacitors conditions

   The output capacitor conditions are defined in the datasheet for output stabilization.
   Does the output capacitor defined here include decoupling capacitors near the load end?

Q2:About Rtrip range

   In the data sheet, the Vtrip range is specified as 0.2V to 3V.
   Since Itrip is 10uA, is the resistance connectable to the TRIP pin in the range of 20kΩ to 300kΩ?
   And,what happens if this condition is not met?

Regards