This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: The firmware version of BQ78350 device

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO

Dear all

      Does the BQ78350-R1 device have 2.02 firmware version ? Or other version ?

      Could you share me what is difference between 2.02 firmware version with 0.00 version ? Thanks a lot.

  • Hi Went,

    The BQ78350-R1 ships with firmware version 1.03. There is version 1.04 on ti.com in the product folder available for download which can be programmed onto the device using the Firmware tab in BQStudio. I recommend updating to the latest firmware.

    There is also firmware for the BQ78350-R2. The latest version is version 2.02. This can also be programmed onto the BQ78350-R1 device. R2 has additional features that may be useful like current scaling and JEITA charge control. 

    Best regards,

    Matt