Hi all,
I have a customer who is looking at using this device for one of his projects. He is monitoring an 8 to 20 V input but because the power supply is subjected to harsh weather conditions he is concerned about performance during surge conditions. They are using external circuitry to handle surges but he wants to make sure in the event of a failure, the rectifier does not draw current in order to protect devices at the load. Has there been any testing to see how the LM74670 fails and can we guarantee him that it will fail as an open?
Thanks!
Stephen