Part Number: BQ34110
Other Parts Discussed in Thread: BQSTUDIO, GPCCEDV
Hello,
The BQ34110 TRM mentions a way to store a remaining capacity value by setting the RESTORE_REMCAP flag in the CEDV Configuration Register in DF: "Upon reset or power-up, the device restores the previous value of RemainingCapacity(), which was stored before going into shutdown". I have tried to make this work but have not had success. I tried changing the DF "Stored Remaining Capacity" value to a different number than the current remaining capacity, then cycling power/resetting, but the remaining capacity number does not change to the stored remaining capacity value. I have also tried using the STORE_REMCAP_A and STORE_REMCAP_B subcommands by using advanced command in BQStudio and writing C1 22 to address 00 or A0 28 to address 00, then reading the DF, but the stored remaining capacity value does not update to the current remaining capacity. Is there a step that I am missing? The TRM has very little information about this.
Thanks,
Colin Yee