This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BQ40Z50-R1 CHG and DSG different ports

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50, BQ78350, BQ76920, BQ34Z100

Can BQ40Z50 be designed as different ports for charging and discharging?

  • Hi

        It is not recommended to use bq40z50 for separated charge and discharge path application. Such applications are very complex and variated, and there could be some customized requirement on FETs control, bq76920 + bq78350 + MCU or bq76920 + bq34z100 + MCU are more suitable, as the MCU can control the FETs directly if it is needed for specific scenario which can not be covered by catalogued bq40z50 device