Hi
I would like to determine the EMI injected by an SMPS to the Mains supply. The challenge is that, i have 2 inputs, one is the Mains AC supply of 230V and the other one is a control signal voltage pulse. When trying to run AC Analysis I get the error "Only one input is allowed". I have attached the file herein. The AC Mains input is VG1 and the signal control is VG2. Should i get rid of the control voltage signal and if so, how will i represent its effects on the SMPS? Kindly guide me on what i can do to determine the EMI as i am still relatively new to TINA.
Kind Regards
SamSMPS.TSC