Hi,
My customer is wondering if the I2C interface can also used 3.3V pull up?
Will there be any risk using 3.3V pull up?
Since 1.8V is mentioned in our datasheet but customer is having 3.3V at their host side.
Great thanks for your help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is wondering if the I2C interface can also used 3.3V pull up?
Will there be any risk using 3.3V pull up?
Since 1.8V is mentioned in our datasheet but customer is having 3.3V at their host side.
Great thanks for your help.
Hello,
1.8V is the minimum pull-up voltage that this device is verified against.
3.3V is fine to use as a pullup rail.
Regards,
Joel H
Hi Joel H,
Please advise digital voltage range spec.(I2C pull-up voltage & CD pin(charger enable/disable), can we control the CD pin with 3.3V level? thanks
Vincent
Hi Joel,
May I know how to define if the I2C interface using 1.8V or 3.3V?
Is there a VIH or VIL threshold for this case?
since I2C interface is usually and open drain structure, 1.8V and 3.3V should be all compatible with each other?
When do we need to use level-shifter ?
Great thanks for your help.
Hello,
The VIH and VIL thresholds for the CD pin are in the EC table of the BQ24158 datasheet.
For the I2C communication, the I2C protocol is standardized. I will refer you to: https://www.i2c-bus.org/ for more information about the I2C protocol. This charger follows the specification listed there.
Regards,
Joel H