Hello Team,
What would the best method to determine when 95% of capacity is used up on the attached battery (Li-SOCL2)? Can the customer read DOD,SOH, current and voltage from the gauge while in the EOS mode and then be able to determine this using an MCU? The application that will be power by this battery will have a wide current draw from uA to 200mA up to an 1A peak currents.