Hi,
My motor drive customer is revisiting ACDC power supply that are 20 years old right now.
They are looking for dual output supply non -isolated input ±18 V ±5%, output ±15 V, 0,1 A.
Any ideas?
Many Thanks,
Antonio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The 18 V comes from an unregulated output of a multi-output switching power supply. The maximum voltage should be slightly higher (5%) than the nominal one, so 30 - 36 V are abundant. The solution does not need to be on a single chip.
Many Thanks,
Antonio
Antonio,
How about two instances of LMR36506/LMR36503?
We can generate the positive output with typical buck and then configure second instance in inverting buck boost configuration for negative output.