Other Parts Discussed in Thread: GPCCHEM
Learning Cycle 102819.zipHi there,
I am still having issues with completing a successful learning cycle with the bq28z610 gas gauge; attached are the log and data memory parameter files for the most recent attempt where I reduced the discharge and charge currents in an attempt to prevent significant cell voltage imbalance. I am using LiFePO4 Tenergy 34009-0 cells setup in a 2S configuration.
I had previously been told that my charging setup was incorrect. I've been attempting the learning cycles using a power supply set to the desired final charge voltage (7.3V) with it current limited to the desired charging current. This appeared to cause problems as the taper current was never achieved and charging current would sometimes go in and out. I was under the impression that the bq28z610 would regulate the charge current itself. Is this true? And what would be the best method for charging the cells?
I also reviewed our data memory parameters and did not find anything that seemed troublesome, but could this also be looked over? Any feedback would be appreciated.
Thanks,
Nick