This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ22010: Can this part and the LMZ23610 be synched to an SSFM clock source?

Part Number: LMZ22010


The requirement is that the part must be able to be synchronized to an external spread spectrum frequency modulated (SSFM) clock source that has it's clock frequency spread over a bandwidth that is +/- 10% of the set frequency.

Do these 2 devices have that capability?

Thanks,
Lauren