In the UCC28950 datasheet section 8.2.2.5 says the maximum power dissipation for clamping diodes Db and Dc is given as = .5*Ls*I^2prms*Fsw
What are the conditions where this worst case power dissipation can occur?
The section in the datasheet says to use MURS360 SMC rectifiers. However, based on the calculation for maximum power dissipation the power can be well over 10 watts which is not going to work with the diodes recommended. Please advise!!
We have observed that certain conditions (abnormally low low output voltage operation) these rectifiers can overheat and fail. Is this expected? How can this be mitigated?