This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support team
may i have your help to compare w/ traditional hard switching full bridge VS phase shift full bridge in 54V input & 1KW application
which one have better efficiency and why?
Hi Red,
The phase shift full bridge offers a zero voltage switching topology and this is results in lower switching losses if the input voltage is high.
For example the UCC28950 is normally used on the 400V output of a pfc stage for this reason.
A 54V full bridge will probably not have a high switching loss.
At 1kW and 54V the conduction losses are going to be more significant than any switching losses.
I am adding a document showing the efficiency of the LM5045 (full bridge) and the LM5046 PSFB and you can see there is very little efficiency changes between these two parts with a 36V to 72V input range.
Regards
John