This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33603: About Inverting buck-boost (IBB) topology

Guru 21045 points
Part Number: LMZM33603


Hi Team,

 

I would like to use LMZM33603 for Inverting buck-boost (IBB) topology.

Then, I understand that I can connect PGND pin and AGND pin.

 

Because, the device has AGND and PGND are internally tied in this device.

Please refer to the following E2E thread.

https://e2e.ti.com/support/power-management/f/196/t/754416?tisearch=e2e-quicksearch&keymatch=LMZM33603

 

Is my understanding correct?

And, could you please let us know if you have any concern?


 

[Supplementary explanation]

By the way, according to datasheet, “Do not connect this pin to PGND”.

This comment is advice for normal operation(buck topology).

Therefore, I understand that it is not applicable in IBB topology.

  

 

Regards,

Hide

  • Hi Hide,

    The recommendation that not connect AGND to PGND is to reduce noise, as your attached discussion.

    Inverting buck-boost has no difference. You don't need to connect them externally.

  • Hi Neal-san,

     

    Thank you for your prompt reply.

    I understand that PGND connect to negative VOUT and AGND connect to Analog GND on board.

    And, this circuit does not have any problem even if the device has AGND and PGND are internally tied in this device.

    Is my understanding correct?

     

    If yes, I have one more question.

    I guess that unnecessary current occurs in the device.

    (From Analog GND (0V) to Negative VOUT(less than 0V).

    Does this current not have any problem?


     

    Regards,

    Hide

  • Hi Hide,

    In your application, both the "IC AGND pin" and "IC PGND pin" should connect to the "system Vout". 

    For your question, I think you want to know if it is needed to connect "IC AGND pin" and "IC PGND pin" externally on pcb board, right? The answer is you don't have to, because they are connected in the IC, and then both of them will connect to the "system Vout". 

    Hope it helps.

  • Hi Neal-san,

     

    Your recognition(my question ) is right.

    And, I'm sorry to confuse you.

     

    I understand that both the "IC AGND pin" and "IC PGND pin" should connect to the "system Vout" in IBB topology.

    (Please refer to the following circuit.)


     

    Regards,

    Hide

  • Hide, let us know if you need more assistance.