Other Parts Discussed in Thread: BQ76930
Dear All
I use bq7963000 + bq78350-r1 device, and the 2.5V power of bq78350-r1 is from REGOUT pin of bq7693000.
When I test the board in environment which is 60 degree and 90% humidity, after 168 hours, I find there are four boards of six boards, which the bq78350-r1 cannot work normal, and the bq7693000 device is very hot, I find the REGOUT pin is only 0.9V, the normal is 2.5V voltage.
1. Did you encounter the similar problem ? How to solve this problem ?
2. If you don't encounter, could you tell what condition that will lead to this problem on the bq78350-r1 ?