Hello team,
Could you please answer my 4 questions?
Q1: The device should turn on above 4.4V because it has 0.4V hysteresis. But in TINA simulation it turned on at 4.5V. Could you explain why there is 0.1V voltage gap?
Q2: Which pin 'current-sense fault condition current' flows? Sense pin? then, it's too high.
Q3: Which pin is the I_sink=5mA flowing? Could you explain about the test condition?
Q4: Is there any method for TPS7B7702-Q1 to check short-to-battery when it doesn't go over threshold voltage?
Thank you.
Regards,
Oliver Kim