Other Parts Discussed in Thread: TPS54302
Hello, I have been using the TPS54302, but finding in the skip/ECO mode (<0.5 A), the ripple is larger than I'd like. Would the TPSM84209 perform better? I do like the lower BOM count on the TPSM84209. Any other pro/cons to consider in comparing these devices?
Vin 14-18V
Vout 5V
Use ranges anywhere between 200mA to 1.25A.